EU Directive 2015/863 restricts the use of the 10 substances listed below in the manufacture of specified types of electrical equipment. Whilst this restriction does not legally apply to components that are supplied by Rapid, we understand that component compliance is relevant to many of our customers and to this end we have created this compliance certificate to assist you in maintaining your records.
This compliance certificate will confirm to our customers that the product in question does not contain any of the restricted substances in concentrations above the permitted level as specified within the directive, excepting those products which are exempt from the directive’s requirements. The restricted substances and their permitted maximum concentrations in any homogenous material by weight are:
Restricted Substance | Maximum Permitted Concentration |
---|---|
Cadmium | 0.01% |
Lead | 0.1% |
Mercury | 0.1% |
Hexavalent Chromium | 0.1% |
PBB (Polybrominated Biphenyls) | 0.1% |
PBDE (Polybrominated Diphenyl Ethers) | 0.1% |
DEHP (Bis(2-ethylhexyl) phthalate) | 0.1% |
BBP (Butyl benzyl phthalate) | 0.1% |
DBP (Dibutyl phthalate) | 0.1% |
DIBP (Diisobutyl phthalate) | 0.1% |
Rapid Electronics Ltd confirms that the supplier of the product listed below has confirmed that the product is RoHS compliant and that reasonable steps have been taken to confirm this statement. This information applies only to products supplied by Rapid Electronics Ltd on, or after the date of this certificate.
Rapid Order Code: 18-0666
Product Description: RECOM R-78W5.0-0.5 DC/DC converter (module) 5 V 500 mA 2.5 W