They offer infrared LED devices commonly used in remote controls, sensors, and night vision systems due to their reliable transmission capabilities. Kingbright LED displays provide clear visual indicators for instrumentation, industrial equipment, and consumer devices. Their photocouplers isolate signals in power supply circuits, providing safe communication between high and low voltage components.
                
                    Kingbright is a world-leading manufacturer of LED components, Kingbright LEDs, and optoelectronic components. Rapid has been an official Kingbright distributor of Kingbright LEDs for more than 30 years, and offers a comprehensive service for customers wishing to buy Kingbright LED components.
As one of Kingbright's leading UK distributors, Rapid can offer excellent rates on high volume orders. The full Kingbright range available from Rapid includes LED displays, surface mount LEDs (SMD LEDs), 3mm, 5mm, 8mm and 10mm through-hole LEDs, light bars and bargraphs, miniature, rectangular, power LED indicators, optics and mounts, clusters, photodetectors, photocouplers, infrared devices and strips, covering a wide variety of electronic components applications.
Founded in Taipei, Taiwan in 1980, Kingbright are at the cutting edge of the fast-moving solid state lighting sector, with a strong reputation for high-performance LED components. There is huge global demand for Kingbright LEDs and related electronic components, and Kingbright constantly strives to meet the designs and demands of their customers, which include international manufacturers of home appliances, security systems, telecommunications equipment, computers, and automotive products.
"The long relationship between Kingbright and Rapid has been critical to the success of Kingbright in the marketplace", says W. J. Song, President of Kingbright Electronics. "This cooperation is built on the fundamental principles of Innovation, Quality, Efficiency and First Class Service, which are shared by both companies and drive our mutual success".
Whatever Kingbright LED you require – even if we do not hold current stock at Rapid – we can source it on short lead times. This is due to our excellent relationship with the manufacturer. Rapid holds stock of a high volume of Kingbright LED components, including SMD LEDs, through-hole LEDs, LED indicators, and LED displays, and with stock arriving regularly, we can provide access to the entire Kingbright portfolio. We can also work with customers on new designs: helping you through the design process with product samples, and offering support with your production, from small volumes all the way through to full-scale production.