You are using beta.rapidonline.com. For the live site go to rapidonline.com

What do I need to build an instrumentation system?

Published on 22 July 26

The short answer

An instrumentation build needs the sensors themselves, signal conditioning, data acquisition where measurements are recorded, screened field cable, M8/M12 connectors, junction boxes, panel-side DIN rail and terminal hardware, a 24V supply, earthing hardware, cable management, loop labelling and tools. The organising idea behind almost all of it is the 4–20mA current loop: current arrives at the far end of a long cable exactly as it left, and the 4mA "live zero" means a dead sensor reads as a fault, not a plausible zero.

  • Define measurement type, range, accuracy and output signal for every loop before selecting a single sensor
  • Screened, twisted-pair cable on every analogue run — and screens earthed at the panel end only
  • Check each transmitter's power architecture: two-wire loop-powered devices need no separate feed, three- and four-wire devices do
  • Segregate instrumentation from power cabling throughout; cross at 90° where routes must meet
  • Tag every cable, terminal and instrument to the loop drawing — unlabelled loops are where commissioning time goes to die

An instrumentation system connects physical measurements — temperature, pressure, flow, position, current — to a control system, data acquisition platform or monitoring network, and getting it right involves far more than choosing sensors. Signal conditioning, cable screening, junction enclosures, earthing and loop labelling all need planning before the first cable is pulled, and they're the categories that stall a commissioning when forgotten. This guide is written for automation engineers, machine builders, process engineers and OEM wiring teams; it doesn't specify part numbers — those follow from your loop schedule — but it covers every category in build order, with links to Rapid's stocked range.

Industrial instrumentation installation with field sensors, junction box and panel-side signal wiring

Why does industrial instrumentation run on 4–20mA?

Because current survives the journey and voltage doesn't. A voltage signal sagged across hundreds of metres of cable arrives smaller than it left, by an amount that depends on cable length, temperature and connection quality — so the reading drifts with the installation. In a series current loop, the same current flows through every point in the circuit regardless of cable resistance: 12mA at the transmitter is 12mA at the panel, full stop. The 4mA floor is the second stroke of genius — a "live zero". A healthy loop reading its minimum value sits at 4mA; a broken wire, dead sensor or failed supply reads 0mA, which is unambiguous fault, not a believable measurement. Voltage-based systems can't tell those two states apart.

The loop also explains the wiring architecture you'll meet in the stages below: a two-wire transmitter powers itself from the loop current, so one screened pair carries both power and signal; the loop is measured in series, which is why a multimeter or clamp meter goes into or around the circuit at commissioning; and what the loop can't defend against — induced interference on top of the signal — is the job of the screening and segregation stages. Once the loop makes sense, the rest of the shopping list stops being arbitrary.

What do you need? The build, stage by stage

1. Field sensors and transducers

Every loop starts at a sensor, and every sensor decision starts with four parameters: what's measured, over what range, to what accuracy, with what output signal. For temperature — the most common industrial measurement — the choice is usually between thermocouples (robust, wide-ranging, self-powered, less accurate) and RTDs such as PT100 (more accurate and stable, but needing excitation), both under temperature sensors. Presence and position are covered by inductive and capacitive proximity sensors, magnetic proximity types, position sensors, ultrasonic sensors for non-contact ranging, and encoders where shafts need speed and position feedback. Process variables take pressure, flow and level sensors; environmental and electrical measurements take humidity, gas and current sensors; and motion rounds out with direction and speed and force sensors. The full sensors range covers the rest.

2. Signal conditioning and isolation

Few sensors speak PLC natively. Signal conditioning converts, amplifies, filters or isolates the raw output into a standard signal — 4–20mA, 0–10V or a digital protocol — with DIN rail transmitters from transmitters and receivers as the standard panel format, supported by interface modules bridging field signals to I/O cards and the wider sensors and monitors range. Where the field circuit must be electrically separated from the control system — hazardous areas, or plants where earth potential differences would corrupt measurements — protection barriers provide intrinsic safety and galvanic isolation, with isolation transformers handling the supply side.

3. Data acquisition and logging

Where measurements need recording — process monitoring, quality assurance, condition monitoring — the data acquisition and logging range covers both ends of the spectrum: standalone loggers recording locally, and networked DAQ systems accepting multiple analogue channels (4–20mA, voltage, thermocouple) and passing digitised values up to SCADA or IIoT platforms.

4. Field wiring and instrumentation cable

The loop protects the signal from resistance; the cable has to protect it from everything else. Analogue runs — especially millivolt thermocouple signals, which have no loop to defend them — use screened, twisted-pair construction from communications and control cables, with multi-pair variants carrying several loops down one route. Standard sensors with M8/M12 ports take pre-terminated sensor cable assemblies — the factory-moulded, tested option — while non-standard runs are cut and terminated on site from the wider cables and wires range.

5. Field connectors

M12 is the field connector of industrial instrumentation: IP67 when mated, tool-free, and keyed by coding — A-coded for general I/O and analogue, D-coded for Profibus and DeviceNet, X-coded for Gigabit Ethernet — with M8 taking over on small sensors where the M12 shell won't fit. The circular connectors range covers assembled connectors, with housings, contacts and accessories for field-wireable terminations. Where cables enter junction boxes and panels rather than mating to a connector, cable glands carry the sealing and strain relief — rated to match the enclosure, or the box's IP rating is fiction.

6. Junction boxes and field enclosures

Rather than running every sensor individually back to the panel, junction boxes marshal local field cables onto terminal blocks and send one multi-pair cable home — fewer routes through the plant, and fault-finding gets a halfway test point. Outdoor and process locations want IP65/IP66 boxes; general purpose enclosures in ABS or polycarbonate cover most duties, heavy duty enclosures handle rougher ones, and GRP earns its premium where chemicals or RF transparency matter. Enclosure accessories and grommets finish the entries. Our enclosure guide covers the material choice in depth.

7. Panel-side termination and DIN rail hardware

At the panel, field cables land on DIN rail terminal blocks mounted on rail from DIN rails and accessories — the same hardware as any control panel, with one instrumentation-specific discipline: screens terminate to dedicated screen terminals, earthed at this end only. Fused terminal blocks give per-loop protection, distribution blocks split the 24V supply across rail sections, barrier strips cover simpler termination duties, and terminal block accessories — end brackets, jumpers and the marker systems the labelling stage depends on — complete the rail. The terminal blocks guide covers the connection-method choice.

8. Power supply

Most transmitters and sensors run on 24V DC from a rail-mounted PSU in the DIN rail power supplies range, sized with 20–30% headroom — but audit the power architecture per device first. Two-wire transmitters draw their power from the loop itself, so they cost the supply at most 20mA each; three- and four-wire devices take a separate feed and dominate the load calculation. Mains reaches the panel through an IEC inlet and equipment connects on leads from power cable assemblies.

9. Earthing and screening hardware

Earth loops between field and panel are the classic source of 50Hz interference on analogue measurements, and the defence is topological: one instrument earth bar, bonded to site earth at a single point, with every screen landed there and floating at the field end. The earthing range covers the bars and bonding hardware; ring terminals terminate bonding conductors at studs and bars, bootlace ferrules dress every stranded conductor entering a terminal, and crimps, splices and terminals covers the remainder. As with the audio world's version of this discipline: manage noise at the screen, never by lifting a safety earth.

10. Cable management and routing

Even well-screened instrumentation cable picks up interference run parallel to drive or motor cables over distance, so segregation is a routing rule, not a preference: separate containment via conduit and trunking, and 90° crossings where instrument and power routes must meet. Cable ties and cable clips secure runs at regular intervals, with sleeving and spiral wrap protecting exposed bundles.

11. Identification and labelling

Every cable, terminal and instrument carries a tag matching the loop drawing — not as good practice but as the thing that makes commissioning and every future fault-finding session possible. Cable markers tag both ends of every run, terminal markers from terminal block accessories number the rail, a label printer produces durable tags matching the as-built documentation, and warning signs and labels cover the statutory markings.

12. Tools

The kit is compact but specific: wire strippers, cutters and pliers for preparation, a ferrule crimper from crimping tools, screwdrivers for terminal and instrument fixings, and — the instrumentation essentials — a multimeter for loop current, continuity and confirming screens aren't accidentally earthed at both ends, plus a clamp meter for verifying loop current without breaking the circuit. Specialist hand tools cover the rest, and a dedicated loop calibrator — sourcing and simulating 4–20mA without a live sensor — repays its cost across the first commissioning.

Complete product checklist

Work through this table against your loop schedule and wiring drawings before ordering — every row covered or consciously ruled out means no stalled commissioning.

Category What you need it for Rapid category
Temperature sensors Process and ambient temperature measurement Temperature sensors / thermocouples
Proximity and position sensors Presence detection and position feedback Proximity / position sensors
Process variable sensors Pressure, flow and level measurement Pressure / flow / level
Encoders Shaft position and speed feedback Encoders
Signal conditioners Converting sensor output to standard 4–20mA or voltage Transmitters and receivers
Interface modules Bridging field signals to PLC I/O Interface modules
Isolation barriers Galvanic isolation; hazardous area intrinsic safety Protection barriers / isolation transformers
Data acquisition Recording and transmitting multi-channel data Data acquisition and logging
Instrumentation cable Screened, twisted-pair signal runs Communications and control cables
Sensor cable assemblies Pre-terminated M8/M12 sensor connections Cable assemblies
M8/M12 connectors IP-rated field connections; check the coding Circular connectors
Cable glands Sealed entry into boxes and panels, rated to match Cable glands and bushes
Junction boxes Marshalling field cables at local points Junction boxes
DIN rail and terminal blocks Panel-side termination with screen terminals DIN rails / terminal blocks
Terminal block accessories End brackets, jumpers, loop markers Terminal block accessories
Fused terminal blocks Per-loop overcurrent protection Fused terminal blocks
DIN rail power supply 24V DC for sensors and transmitters, with headroom DIN rail power supplies
Earthing hardware Instrument earth bar and bonding terminations Earthing / ring terminals
Bootlace ferrules Every stranded conductor into screw terminals Bootlace ferrules
Conduit and trunking Routing and segregation from power cabling Conduit and trunking
Cable ties and clips Securing field cable runs Cable ties / cable clips
Loop identification Cable, terminal and instrument tags to the loop drawing Cable markers / label printers
Multimeter and clamp meter Loop current, continuity and screen checks Multimeters / clamp meters
Hand tools Strippers, cutters, ferrule crimper Pliers and cutters / crimp tools

Ordering and despatch: high-volume lines across every category in this guide — sensors, signal conditioners, terminal blocks, cable, connectors and tools — are ready to order, with same-day despatch on UK-stocked items and delivery within a week for extended-range stock. Contact Rapid to discuss specialist requirements.

Source everything for your instrumentation system from a single supplier, with same-day despatch on UK-stocked lines.

Browse sensors and instrumentation

Frequently asked questions

What is the difference between a two-wire and a four-wire transmitter?

A two-wire transmitter powers itself from the 4–20mA loop, so one pair carries both power and signal. A four-wire transmitter takes a separate 24V feed alongside its signal output. Two-wire wiring is simpler and cheaper; four-wire is needed where the device draws more power than a loop can supply or must output a voltage signal.

Why do instrumentation cables need to be screened?

Industrial plants are electromagnetically noisy — drives, contactors and power cabling all induce interference, and analogue signals (especially millivolt thermocouple levels) are small enough to be corrupted by it. A screen intercepts induced currents and diverts them to earth. Land the screen at one end only; earthing both ends creates a loop that can make things worse.

What is a protection barrier and when do I need one?

Protection barriers — Zener barriers and galvanic isolators — connect instruments in hazardous areas to control equipment in safe areas by limiting the energy entering the hazardous zone below ignition levels (intrinsic safety). Galvanic types also fully isolate field from control circuits, eliminating earth loops. ATEX/IECEx regulations require them wherever sensors sit in classified zones.

What do the M12 connector codings mean?

The coding letter fixes the pin arrangement and keying so incompatible systems can't mate: A-coded for general I/O and analogue signals, B-coded for legacy fieldbus, D-coded for Profibus/DeviceNet, X-coded for Gigabit Ethernet. Match the coding to the device port when ordering from the circular connectors range — the thread is the same, the key isn't.

Related guides and categories

What do I need to build a control panel? · Terminal blocks: how to choose · Choosing the right enclosure · Sensors · Data acquisition and logging · Automation and control

Share

Post a Comment



Trustpilot