You are using beta.rapidonline.com. For the live site go to rapidonline.com

Understanding K-type thermocouples

Published on 09 July 26

The K-type is the general-purpose workhorse of temperature measurement: a chromel–alumel thermocouple covering roughly −200°C to +1260°C, cheap to make, tough enough for industrial use and supported by practically every meter, logger and controller on the market. If a piece of equipment has a thermocouple input and doesn't say otherwise, it's expecting a K-type.

This guide explains how thermocouples actually work, what the K-type's range and accuracy classes mean in practice, how to read the IEC and ANSI colour codes without falling into the classic polarity trap, which junction style suits which job — and, just as usefully, the situations where a K-type is the wrong answer.

How does a thermocouple work?

Join two different metals at one end, put that junction somewhere hot or cold, and a small voltage appears across the free ends — the Seebeck effect. The voltage depends on the temperature difference between the measuring junction and the point where the wires meet the instrument, which is why every thermocouple reading involves a second measurement you never see: the meter senses its own terminal temperature and adds it back in, a step called cold junction compensation.

Two practical consequences follow. First, a thermocouple has no absolute accuracy of its own — the instrument's compensation is part of the measurement chain. Second, the signal is tiny: a K-type produces about 41 microvolts per degree, so wiring practice, connections and electrical noise all matter far more than they would for a sensor with a healthy output signal.

What is a K-type made of, and what range does it cover?

The positive leg is chromel (a nickel–chromium alloy) and the negative leg is alumel (nickel with aluminium, manganese and silicon). Between them they cover a nominal −200°C to +1260°C — though the usable continuous maximum depends heavily on wire diameter and sheath: fine-gauge bare wire degrades far sooner than a heavy mineral-insulated probe, so treat the headline figure as the ceiling of the type, not of every probe made from it.

Accuracy is defined by tolerance class under IEC 60584, and the numbers are worth internalising because they're larger than newcomers expect:

Tolerance class Tolerance In practice at 500°C
Class 1±1.5°C or ±0.4% of reading, whichever is greater±2°C
Class 2±2.5°C or ±0.75% of reading, whichever is greater±3.75°C

Add the instrument's own error and cold junction compensation on top, and a routine K-type measurement is honestly a couple-of-degrees affair. For most process, oven and workshop measurement that's exactly good enough; where it isn't, the answer is a different sensor type, covered below.

What do the colour codes mean?

Thermocouple types are identified by colour, but two coding systems are in circulation and they disagree with each other in the worst possible way.

Standard Overall / connector Positive leg Negative leg
IEC 60584-3 (UK/EU)GreenGreenWhite
ANSI MC96.1 (US)YellowYellowRed

The trap is the American red wire: in ANSI colour coding, red is the negative leg — the exact opposite of every other electrical convention. Connect a US-coded thermocouple by instinct and the reading moves the wrong way as temperature rises. UK-supplied probes and connectors follow the IEC green scheme, but imported equipment and US-authored documentation keep the yellow system alive, so both are worth recognising on sight.

Which junction type should you choose?

Sheathed probes come with the measuring junction built one of three ways, trading speed against protection:

  • Exposed junction — the fastest response, because the junction sits in direct contact with the medium, but it's fragile and unsuitable for conductive liquids or corrosive environments
  • Grounded junction — welded to the inside of the sheath tip, giving good response with full mechanical protection; the catch is an electrical path from the process to the instrument, which can create ground loops and noise in electrically hostile installations
  • Ungrounded (insulated) junction — isolated from the sheath, slower to respond but electrically clean, and the safe default when the probe touches machinery, heaters or anything else at an uncertain potential

For panel and process installations feeding instrumentation, panel meters or PID controllers, the ungrounded style avoids a whole category of baffling intermittent faults for the cost of a second or two of response time.

When is a K-type the wrong choice?

The K-type's weaknesses are as well documented as its strengths, and an honest selection guide names them. In low-oxygen or reducing atmospheres between roughly 800°C and 1050°C, the chromel leg suffers preferential oxidation known as green rot, drifting the calibration steadily downwards — sealed furnaces and kilns are the classic scene of the crime. For sustained high-temperature work, the N-type was developed specifically to resist the drift mechanisms that age K-types, at a modest cost premium and with equally wide instrument support.

Below about 150°C the competition changes character. A PT100 resistance sensor offers fraction-of-a-degree accuracy and long-term stability no thermocouple can match, and a thermistor resolves hundredths of a degree over a narrow span — which is why battery packs and onboard monitoring use them rather than thermocouples. The honest hierarchy: thermocouples win on range, robustness and price; resistance sensors win on accuracy; sensor ICs win on convenience in embedded designs. The K-type's dominance comes from being good enough at almost everything, not best at anything.

How do you get accurate readings in practice?

Most K-type problems are installation problems. The rules that prevent them:

  • Extend with K-type cable only. Every wire in the chain back to the instrument must be thermocouple material — splice in ordinary copper and you create new junctions that add their own voltages. Compensating cable and K-type connectors exist for exactly this reason
  • Immerse the probe properly. A tip barely inserted into a process conducts heat away along the sheath and reads low; a common rule is immersion of at least several times the sheath diameter
  • Keep signal away from power. Microvolt signals and mains cables don't share trunking happily; route thermocouple runs separately and use screened cable where noise is unavoidable
  • Check against a reference. A periodic comparison at a known temperature — melting ice at 0°C is the classic field reference, or a dry block from the calibrator tools range for anything traceable — catches drift before it corrupts weeks of logged data

For handheld work, any decent thermocouple thermometer handles the cold junction compensation invisibly; the discipline above is about making sure the signal arriving at it still means what the probe measured.

Featured temperature measurement

Frequently asked questions

What temperature range does a K-type thermocouple cover?

Nominally −200°C to +1260°C. The continuous maximum for a specific probe depends on its wire gauge and sheath — fine bare-wire types degrade well below the headline figure, while mineral-insulated probes approach it. Check the probe's own rating, not just the type's.

What do the colours on a thermocouple connector mean?

They identify the type: green is K-type under the IEC scheme used in the UK and Europe; a yellow connector is K-type under the US ANSI scheme. On US-coded wire, red is the negative leg — opposite to normal electrical convention.

Can I extend a thermocouple with ordinary wire?

No. Copper extensions create new metal-to-metal junctions that generate their own voltages and corrupt the reading. Use K-type or K-compensating cable and K-type connectors for the entire run back to the instrument.

Should I choose a grounded or ungrounded probe?

Ungrounded is the safe default: it isolates the instrument from the process electrically, avoiding ground loops, at the cost of slightly slower response. Grounded probes respond faster and suit electrically quiet installations; exposed junctions are fastest but fragile.

Why is my K-type reading drifting low over time?

If the probe lives in a sealed or low-oxygen environment at high temperature, suspect green rot — selective oxidation of the chromel leg that progressively lowers readings. Improving ventilation, shortening exposure or switching to an N-type are the standard fixes.

How accurate is a K-type thermocouple?

Class 1 tolerance is ±1.5°C or ±0.4% of reading, Class 2 is ±2.5°C or ±0.75%, and the instrument adds its own error on top. For accuracy much better than a degree or two, a PT100 resistance sensor is the more appropriate tool.

Measure with confidence

From general-purpose bead probes to mineral-insulated industrial sensors, with the meters, loggers and calibration references to trust what they tell you.

Browse thermocouples and probes View thermometry range
Share

Post a Comment



Trustpilot