You are using beta.rapidonline.com. For the live site go to rapidonline.com

NE555P alternatives and equivalents: what to use instead

Published on 06 July 26

The Texas Instruments NE555P is the standard bipolar 555 timer in a DIP-8 package, probably the most recognisable IC part number in electronics, and still in volume production more than fifty years after the original design. People usually look for an alternative for one of three reasons: they need lower supply current, they need two timers in one package, or they simply want to know what else does the same job. All three have good answers in current production parts.

Short answer

For most NE555P circuits, the TI TLC555CP is the closest pin-compatible substitute, same DIP-8 pinout, wider 2–18 V supply range and a fraction of the supply current. The ICM7555IPA is the equivalent CMOS option from Intersil. The one check that matters before swapping: CMOS versions cannot sink or source the 200 mA the bipolar NE555P can, so circuits driving relays, motors or high-current LEDs directly from pin 3 should stay bipolar.

How the alternatives compare

All four parts below share the same core timing behaviour - the familiar two-comparator, flip-flop and discharge transistor arrangement, with timing set by an external resistor and capacitor. The differences that decide a substitution are supply current, output drive and maximum oscillation frequency.

Part Technology Supply range Typical supply current Output drive Package
NE555P Bipolar 4.5–16 V ~3 mA at 5 V Up to 200 mA sink or source DIP-8
TLC555CP LinCMOS 2–18 V ~170 µA at 5 V ~100 mA sink, ~10 mA source DIP-8
ICM7555IPA CMOS 2–18 V ~60 µA at 5 V ~100 mA sink, lower source DIP-8
NE556N Bipolar, dual 4.5–16 V ~6 mA at 5 V (both timers) Up to 200 mA per output DIP-14

Which alternative is a direct drop-in for the NE555P?

The TLC555CP uses the same DIP-8 pinout, so in most timing and oscillator circuits it drops straight into the NE555P's socket with no layout changes. It brings some genuine advantages beyond compatibility: it runs from as little as 2 V, draws microamps rather than milliamps, and oscillates reliably to around 2 MHz where the bipolar part becomes unreliable well below that. Because its threshold and trigger inputs draw almost no current, it also tolerates much larger timing resistors - into the tens of megohms - which means long delays can be built with smaller, cheaper capacitors.

The ICM7555IPA occupies the same ground. It is the original CMOS re-implementation of the 555 and behaves near identically to the TLC555 in practice; choosing between the two usually comes down to availability and price rather than any circuit-level difference.

One behavioural difference works in the CMOS parts' favour: the bipolar NE555P draws a brief, heavy current spike from the supply each time its output switches, which is why a substantial decoupling capacitor close to the IC is standard practice. The CMOS versions largely eliminate this, making them better behaved on shared supply rails alongside sensitive analogue or logic circuitry.

When should you stay with the bipolar NE555P?

Output drive is the deciding factor. The NE555P can sink or source up to 200 mA, which is why so many published circuits drive relays, small motors, buzzers and LED clusters directly from pin 3. The CMOS parts sink around 100 mA at best and source considerably less, so a circuit that relies on the bipolar part's muscle will underperform or simply not work - with a CMOS substitute unless a transistor buffer is added.

The other reason to stay put is a validated design. Where a timing circuit has been proven around the bipolar part's characteristics, its output saturation voltages, its supply behaviour, its temperature response - the lowest-risk option is like-for-like replacement. The NE555 remains an actively manufactured, multi-sourced part, so there is no obsolescence pressure forcing a change.

What if you need two timers?

The NE556N puts two independent bipolar 555s into a single DIP-14 - electrically identical timers sharing only power and ground, commonly used where a monostable triggers an astable or two timing stages run side by side. It is not a pin-compatible substitute for a single NE555P, so it suits new layouts rather than rework. The CMOS equivalent is the TLC556CN, which pairs two LinCMOS timers in the same DIP-14 footprint.

What should you check before substituting?

Four things cover almost every case. First, output loading - anything drawing more than a few tens of milliamps from pin 3 needs the bipolar part or an added driver stage. Second, supply voltage - all the parts here overlap between 4.5 and 16 V, but only the CMOS versions run below that, and only they are rated to 18 V. Third, timing components - existing R and C values carry over directly, though CMOS versions open up higher resistor values if you want them. Fourth, frequency - above roughly 100 kHz the CMOS parts are the safer choice, not just an acceptable one.

555 timers for teaching and project work

The 555 remains the standard introduction to timing circuits in schools and colleges, and complete project builds are often more practical than loose components. The Rapid 555 astable/monostable project pack covers both classic configurations in a five-board classroom pack, and RK Education's 555 astable project offers a lower-cost single-board route to the same learning outcomes.

Browse the full timer IC range

Single and dual 555 timers, CMOS low-power versions and signal generator ICs.

Frequently asked questions

Is the TLC555 a drop-in replacement for the NE555?

In most circuits, yes - it shares the DIP-8 pinout and timing behaviour, and existing resistor and capacitor values carry over unchanged. The exception is any circuit driving more than around 100 mA from the output, where the bipolar NE555P's stronger drive is still needed.

What is the difference between the NE555 and the ICM7555?

The ICM7555 is a CMOS version of the same timer. It draws roughly fifty times less supply current, runs from 2–18 V rather than 4.5–16 V, and avoids the supply current spikes the bipolar part produces when switching - but it cannot drive heavy loads directly.

Can an NE556 replace two NE555s?

Electrically, yes - the NE556N contains two independent timers identical in behaviour to the NE555. Physically it is a DIP-14 rather than two DIP-8s, so it suits new designs and consolidated layouts rather than direct board rework.

Is the NE555 obsolete?

No. The 555 is still manufactured in volume by several semiconductor makers and remains one of the most widely used ICs ever produced. Alternatives are usually chosen for lower power consumption or specific circuit needs, not because the original is going away.

Share

Post a Comment



Trustpilot