You are using beta.rapidonline.com. For the live site go to rapidonline.com

News

26 August 26

Why suppliers and brands enjoy working with Rapid

Great supplier relationships are a big part of how we help customers get the right result. At Smart Manufacturing Week, three of the brands we work with — FLIR, Brainboxes and CRC Indu...Read the full story

26 August 26

The own brands behind your next build

Alongside the thousands of exceptional products we stock at Rapid, we also design and back our own exclusive brands — giving you great-value options across a huge range of categories...Read the full story

07 August 26

What is a logic gate? Types, families and how to choose

Short answer A logic gate is a building block of a digital circuit that takes one or more binary inputs (0 or 1) and produces a single binary output according to a fixed rule. The seven core ga...Read the full story

04 August 26

PID control essentials for industrial automation

PID control is how machines hold a value steady against a world that keeps disturbing it — the oven at temperature as the door opens, the motor at speed as the load bites, the pressure constant as dem...Read the full story

04 August 26

Cable assemblies: a complete guide

The short answer A cable assembly is a cable terminated with connectors at one or both ends — a finished, tested, plug-and-play part rather than raw cable to be cut and terminated on the bench....Read the full story

30 July 26

Fibre optic cables: single-mode vs multimode

Fibre optic cable carries data as light down a glass core, guided by total internal reflection — the same physics demonstrated with a torch and a water stream in every school lab, industrialised into ...Read the full story

30 July 26

UPS systems and the role they play in power protection

An uninterruptible power supply does a more modest job than its name suggests, and understanding that is the key to buying the right one. A typical UPS exists to bridge the gap between the mains faili...Read the full story

29 July 26

Solder and flux explained: alloys, types and how to choose

Joint quality is decided by three things: the iron, the technique and the consumables — and the third gets the least attention while causing a remarkable share of the problems. The solder alloy sets t...Read the full story

28 July 26

PCB design basics: layout rules and prototyping routes

A printed circuit board is a laminate sandwich: a fibreglass substrate (almost always FR-4), copper foil etched into tracks, a solder mask that keeps molten solder where it belongs, and a silkscreen l...Read the full story

28 July 26

18650 batteries: the specs that actually matter

The 18650 is the workhorse lithium-ion cell — 18mm across, 65mm long, and behind everything from torches and vapes to power tool packs, e-bikes and portable instruments. The catch is that every 18650 ...Read the full story

27 July 26

Understanding potentiometers and how they work

A potentiometer is a resistor with a third terminal — a wiper that slides along the resistive track — and that one addition makes it two components in one. Use all three terminals and it's a voltage d...Read the full story

27 July 26

Connectors: types and how to choose

The short answer Choose a connector by asking why the joint needs to separate at all. Every connector is a deliberately engineered break in a circuit — added to make a product easier to build, ...Read the full story

22 July 26

Circuit breakers explained: MCBs, RCDs and RCBOs compared

The three devices in a modern consumer unit or control panel divide the protection job neatly: an MCB protects the circuit against overcurrent, an RCD protects people against earth leakage, and an RCB...Read the full story

22 July 26

What do I need to build an instrumentation system?

The short answer An instrumentation build needs the sensors themselves, signal conditioning, data acquisition where measurements are recorded, screened field cable, M8/M12 connectors, junctio...Read the full story

17 July 26

Contactor selection for motor switching

Undersized contactors are one of the most common causes of premature failure in motor circuits — and the mistake usually happens at specification, not installation, because the headline current rating...Read the full story

16 July 26

Thermocouple vs RTD vs thermistor: how to choose

Choose a thermocouple for wide temperature ranges and harsh environments, an RTD for accuracy and long-term stability, and a thermistor for high sensitivity over a narrow range at low cost. That's the...Read the full story

Someone assembling cables 16 July 26

How to choose the right cable or wire for your application

Choosing the right cable or wire doesn’t have to be complicated, but it does mean knowing what actually matters for your specific setup. Rather than looking at everything at once, it’s easier to bre...Read the full story

15 July 26

Bolt and screw size guide: metric charts, spanner sizes and thread basics

A metric fastener designation reads diameter × pitch × length: M6 × 1.0 × 20 is a 6 mm nominal diameter thread with a 1.0 mm pitch, 20 mm long. Drop the pitch — M6 × 20 — and the standard coarse pit...Read the full story

15 July 26

L7805CV alternatives: 7805 equivalents compared

The ST L7805CV is the standard three-terminal 5V linear regulator — the TO-220 part that has turned unregulated supplies into clean 5V rails for fifty years. It isn't going anywhere: the 7805 remain...Read the full story

14 July 26

Resistor colour codes explained: how to read 4, 5 and 6-band resistors

Resistor colour bands encode the value directly: the first bands are digits, the next is a multiplier, and the last is the tolerance. Yellow–violet–red–gold reads as 4, 7, ×100 — 4.7 kΩ at ±5%. Ten co...Read the full story

13 July 26

What do I need to build a control panel?

The short answer A control panel build needs ten categories of product: enclosure, DIN rail, power supply and distribution, control devices, terminal blocks, internal wiring, cable management, ...Read the full story


Trustpilot