You are using beta.rapidonline.com. For the live site go to rapidonline.com

Understanding potentiometers and how they work

Published on 27 July 26

A potentiometer is a resistor with a third terminal — a wiper that slides along the resistive track — and that one addition makes it two components in one. Use all three terminals and it's a voltage divider, turning shaft position into a proportional voltage: the volume control, the sensor, the setpoint knob. Use just the wiper and one end and it's a rheostat, a plain variable resistance. Same part, different wiring, and knowing which job you're asking of it decides everything else about choosing one.

This guide covers how pots work in both roles, what the taper letters actually mean on modern parts, the difference between panel controls and set-and-forget presets, the materials that decide feel and lifespan, the ratings that catch people out — and when the right answer is an encoder instead.

Potentiometer or rheostat: what's the difference?

Wiring, not hardware. Connected as a divider — signal or supply across the two track ends, output taken from the wiper — the pot outputs a fraction of its input set by shaft position, which is how volume controls, joystick axes and position sensors work. Connected as a rheostat — wiper plus one end in series with a load — it simply varies resistance, throttling current for a lamp dimmer or a motor trim.

One professional habit worth copying for rheostat use: also connect the wiper to the unused track end. It changes nothing in normal operation, but if the wiper ever loses contact on a worn or dirty track, the circuit sees the full track resistance instead of going open — a degraded setting rather than a dead one. In control circuits that fail-safe distinction matters.

What do the taper letters mean?

The taper is how resistance is distributed along the track — and it's the specification most often bought wrong. A linear taper changes resistance evenly with rotation: half-way is half the value. A logarithmic (audio) taper bunches its change toward one end, matching the logarithmic way human hearing perceives loudness — which is why a volume control needs one. Put a linear pot in a volume position and all the useful action crams into the first quarter-turn, with the rest doing almost nothing audible.

On the letter codes, a caution born of history: on most modern parts — following the marking convention that now dominates — B means linear (B10K is a 10 kΩ linear pot) and A means logarithmic (A10K for audio). Older American-made equipment used the letters the other way around. When restoring or repairing, trust the behaviour, not the letter: measure wiper-to-end resistance at half rotation — near half the total value means linear, far from it means log.

Panel pots, presets and trimmers

The mechanical duty divides the family. Control potentiometers are built for fingers: rated for tens of thousands of rotations or more, with bushings and shafts that take knobs and daily use. Preset potentiometers — trimmers — are built for a screwdriver a handful of times: they set a bias, a calibration or a threshold at build time and then hold it, with adjustment lives measured in hundreds of cycles, not thousands. Using a preset as a user control wears it out in weeks; the two look related and are engineered for opposite lives.

Within presets, multi-turn cermet trimmers are the precision option — 12 or 25 turns of screw driving the wiper through its travel turns a twitchy single-turn adjustment into something settable to a fine fraction of the range, which is why calibration points on instruments use them. An insulated trimmer tool rather than a metal screwdriver keeps your hand's capacitance and an accidental short out of a live adjustment. For front panels wanting travel instead of rotation, slide potentiometers are the same electrical component on a straight track — the mixing-desk fader — and dial types integrate the readout into the control.

What are the tracks made of, and why does it matter?

Track material sets feel, noise and lifespan. Carbon is the economy choice — perfectly serviceable, but it wears and gets electrically noisier with age. Cermet (ceramic-metal) is stable and durable, the default in quality trimmers. Conductive plastic offers the smoothest travel and the longest rotational life, which is why it owns faders and precision panel controls. Wirewound tracks handle real power and achieve low resistance values, at the cost of resolution that steps from turn to turn of the winding rather than sweeping continuously — fine for a load bank, wrong for audio.

Which ratings catch people out?

Two, reliably. The power rating applies to the whole track — use a pot as a rheostat with only a fraction of the track in circuit and that fraction can only dissipate its proportional share. A 0.5 W pot dialled down to a tenth of its track is a 0.05 W resistor at that setting, and the burnt patch near one end of a failed rheostat is this rule enforcing itself. Second, the wiper has its own current limit, usually far below what the track's power rating implies — divider circuits, where the wiper feeds a high-impedance input and carries almost nothing, are the component's natural habitat; rheostat duty at real current needs a part rated for it, or a wirewound built for the job.

Beyond those: resistance value (for dividers, the value sets the load on the source and the noise floor more than the function — 10 k is the versatile default), taper as above, and tolerance, which on ordinary pots is a relaxed ±20% because absolute value rarely matters in a component you adjust by ear or by eye.

What about rotary encoders?

Where the knob talks to a microcontroller — especially in high-cycle or continuous-rotation duty — a rotary encoder is often the modern replacement, trading the pot's instant analogue simplicity for digital feedback with no track to wear. The full engineering trade-off deserves its own discussion, and gets one in our guide to potentiometers vs rotary encoders. The short version: the pot keeps every job where genuine analogue behaviour matters — real-time voltage division, processor-free circuits, absolute position known at power-up — with digital potentiometer ICs occupying the middle ground for software-controlled adjustment.

Featured potentiometers and controls

Frequently asked questions

What's the difference between a potentiometer and a variable resistor?

A potentiometer used with all three terminals is a voltage divider; wired with two terminals it acts as a variable resistor (rheostat). The names describe the wiring and the job — the physical component is the same.

What does B10K mean on a potentiometer?

On modern parts, a 10 kΩ linear-taper pot; A10K would be the 10 kΩ logarithmic (audio) version. Older American equipment used the letters the opposite way, so on vintage gear verify by measuring resistance at half rotation rather than trusting the letter.

Should a volume control be linear or logarithmic?

Logarithmic. Hearing perceives loudness logarithmically, so a log taper makes volume feel even across the rotation. A linear pot in a volume position concentrates the entire audible change into the first fraction of travel.

Why is my volume pot crackly?

A worn or dirty track, or DC leaking onto the wiper from a failing coupling capacitor upstream — the classic amplifier fault. Contact cleaner buys time on a dirty track; a scratchy pot that returns quickly usually means the DC problem, or a track worn past cleaning.

Can I use a preset trimmer as a front-panel control?

Not for long. Presets are rated for a few hundred adjustment cycles — set-and-forget duty — against tens of thousands or more for proper panel potentiometers. As a daily-use control, a trimmer wears out in weeks.

How much power can a potentiometer handle?

Its rating applies to the full track. Used as a rheostat with part of the track in circuit, the usable dissipation shrinks proportionally — a 0.5 W pot at a tenth of its travel is a 0.05 W resistor. For real current, use wirewound types rated for rheostat duty.

Take control

From panel pots and faders to multi-turn trimmers and encoders, with the knobs and tools to finish the front panel properly.

Browse potentiometers View control potentiometers
Share

Post a Comment



Trustpilot