You are using beta.rapidonline.com. For the live site go to rapidonline.com

Single board computers at the edge: from prototyping to deployment

Published on 24 February 26
Close up of a CPU

Single board computers (SBCs) were once associated primarily with education, hobby projects and early-stage prototyping. Today, that perception is rapidly changing. Advances in processing power, connectivity, reliability and industrial design mean SBCs are increasingly deployed in commercial, industrial and embedded edge environments. The modern industrial SBC is a master of efficiency, capable of driving complex edge computing architectures that were once the sole domain of bulky industrial PCs.

From edge AI inference to robotics control and remote monitoring, modern SBCs are now being selected not just for experimentation, but for long-term operational deployment. As organisations push more processing toward the edge, SBCs are emerging as a practical alternative to traditional industrial PCs in many applications.

The evolution of single board computers

Early SBC adoption was driven largely by accessibility and cost. Developers and students used them to:

  • Learn programming and electronics
  • Prototype embedded applications
  • Build proof-of-concept systems
  • Test IoT connectivity

However, the latest generation of SBCs has evolved significantly. Improvements now include:

  • Multi-core processors capable of running full operating systems
  • Hardware acceleration for AI and vision workloads
  • Gigabit networking and wireless connectivity
  • Expanded industrial I/O interfaces
  • Improved thermal management options

These advancements mean SBCs can now support production-ready workloads, not just development experiments.

As a result, the conversation around SBCs has shifted from “Can we prototype with this?” to “Can we deploy this reliably at scale?”

Why edge computing is driving SBC adoption

The growth of edge computing is one of the main factors accelerating SBC deployment.

Instead of sending all data to central servers or cloud platforms, many systems now process information locally to achieve:

  • Lower latency
  • Reduced bandwidth usage
  • Improved reliability during network outages
  • Enhanced data privacy and security

SBCs are well suited to edge roles because they combine:

  • Compact physical footprint
  • Relatively low power consumption
  • Sufficient processing performance
  • Flexible connectivity

This balance makes them ideal for installations where a full industrial PC would be oversized, costly, or power-hungry.

Edge computing background

SBC use cases in modern industrial and commercial systems

Edge AI and machine vision

SBCs equipped with GPU or AI accelerator support are increasingly used for:

  • Object detection on production lines
  • Quality inspection systems
  • Smart retail analytics
  • Access control and facial recognition
  • Predictive maintenance monitoring

Running AI inference locally reduces response times and allows systems to operate even when cloud connectivity is limited.

When selecting a single board computer for AI, engineers must look beyond raw CPU clock speeds. Modern edge AI workloads rely on integrated NPUs (Neural Processing Units) to handle real-time inference for object detection and predictive maintenance.

Robotics and motion control

In robotics applications, SBCs are often deployed as:

  • Central control nodes for autonomous robots
  • Interfaces between sensors and motor controllers
  • Navigation processing units
  • Communications gateways

Their ability to run Linux-based environments while interfacing directly with GPIO, serial buses, or industrial protocols makes them highly adaptable for robotic platforms.

Industrial monitoring and IoT gateways

SBCs are widely used in:

  • Environmental monitoring stations
  • Energy metering systems
  • Remote asset tracking
  • Factory equipment diagnostics
  • Smart building infrastructure

In these roles, they act as edge gateways, collecting data from sensors and transmitting processed information upstream while maintaining local control logic.

How to choose a single board computer for AI and machine learning tasks?

To choose a single board computer for AI, first determine the required hardware acceleration. Evaluate performance using Trillions of Operations Per Second (TOPS) for integer math, matching the board’s capacity to your specific model complexity. You must also ensure software compatibility. Consider your power budget, as integrated NPUs are better for battery-powered IoT devices, while high-performance GPUs may require active cooling solutions. Finally, verify that the board’s memory bandwidth and I/O interfaces meet the throughput needs of your application.

Robots working on single board computers

Reliability and industrial suitability

One of the historic concerns around SBC deployment was reliability in demanding environments. Modern industrial-oriented SBC designs increasingly address this through:

Extended operating ranges

Many SBCs now support wider temperature tolerances suitable for factory floors, outdoor installations, or transport systems.

Storage flexibility

Support for industrial-grade flash storage, eMMC, or SSD options improves system durability compared with consumer-grade media.

Long-term availability

Industrial SBC vendors often offer extended product lifecycles, helping organisations avoid redesigns caused by discontinued hardware.

Thermal and mechanical options

Passive cooling designs, rugged enclosures and DIN-rail mounting compatibility allow SBCs to integrate more easily into control cabinets and industrial housings.

These factors are helping position SBCs as stable embedded platforms, not just development boards.

How do eMMC and NVMe storage improve SBC reliability over SD cards?

Standard microSD cards are the leading cause of SBC failure due to limited write cycles and vibration sensitivity. Industrial deployments in 2026 prioritise eMMC (embedded Multi-Media Controller), which is soldered directly to the board for better shock resistance, or NVMe M.2 SSDs (via PCIe lanes). These storage methods offer significantly higher TBW (Total Bytes Written) ratings and power-loss protection, preventing the "OS corruption" common in SD-card-based systems during sudden power outages.

I/O Flexibility: A key advantage over traditional PCs

One of the strongest arguments for SBC adoption in embedded systems is their direct hardware interface capability.

Unlike conventional desktop or industrial PCs, SBCs frequently include:

  • GPIO pins for direct signal control
  • I²C, SPI and UART interfaces
  • CAN bus support
  • PWM outputs for motor or actuator control
  • camera and display interfaces

This allows engineers to connect sensors, controllers and peripherals without additional interface cards or converters.

For embedded designs, this can mean:

  • Simpler system architecture
  • Reduced component count
  • Lower power consumption
  • Faster integration timelines

In many cases, SBCs provide the embedded control flexibility of microcontrollers combined with the computing power of full operating systems.

Why SBCs are often chosen over traditional PCs

While industrial PCs remain essential in high-performance or mission-critical environments, SBCs are increasingly preferred when:

Space is limited

Their compact footprint allows installation inside equipment, kiosks, robots, or control panels.

Power efficiency matters

Lower energy consumption reduces thermal management needs and operating costs.

Custom integration is required

Direct hardware interfaces enable tighter integration with sensors, actuators and embedded subsystems.

Cost scalability is important

For multi-unit deployments, SBCs can significantly reduce per-device hardware costs.

Edge deployment is distributed

When dozens or hundreds of small processing nodes are required, SBCs offer a practical and scalable approach.


This combination makes SBCs particularly attractive for embedded edge computing architectures.

From prototype to production: what organisations should consider

Moving from proof-of-concept to deployment with SBCs requires planning beyond initial functionality.

Key considerations include:

  • Operating system stability and update strategy
  • Enclosure design and environmental protection
  • Power supply reliability and redundancy
  • Remote monitoring and device management
  • Security hardening for network-connected systems

Addressing these factors early helps ensure that an SBC-based solution can transition smoothly from development into long-term operational service.

The future role of SBCs in embedded systems

As processors become more efficient and AI acceleration becomes standard, SBCs are expected to play an even larger role in:

  • Distributed edge intelligence
  • Autonomous systems
  • Industrial automation nodes
  • Smart infrastructure deployments
  • Connected monitoring platforms

Rather than replacing industrial PCs entirely, SBCs are increasingly filling the space between:

  • Low-power microcontroller systems
  • Full-scale industrial computing platforms

This middle ground is expanding quickly, making SBCs one of the most versatile building blocks in modern embedded design.

Final thoughts

Single board computers have evolved far beyond their origins in classrooms and hobby projects. With improved performance, connectivity and industrial-ready features, they are now widely deployed in edge AI, robotics, monitoring and embedded control applications. Whether you are deploying a single board computer for AI to monitor factory safety or using an industrial SBC as a rugged gateway, these devices represent the future of edge computing.

For many organisations, SBCs offer the right balance of computing capability, hardware flexibility and deployment efficiency — enabling systems that are compact, scalable and well suited to distributed edge environments.

As edge computing continues to grow, SBCs are no longer just prototyping tools. They are becoming core infrastructure components in modern industrial and commercial technology stacks. And as an approved Raspberry Pi industry reseller, Rapid is here to support organisations in selecting and deploying reliable SBC platforms built for sustained industrial performance.

Share

Post a Comment



Trustpilot