You are using beta.rapidonline.com. For the live site go to rapidonline.com

Maximising uptime: the engineer’s guide to standardised cable selection

Published on 01 May 26

In a high-throughput electronics manufacturing environment, the cable is often the most overlooked component - until it fails. A single fractured core or a compromised shield can halt a production line, leading to thousands of pounds in lost revenue. Standardising your cable selection isn't just about tidying up your BOM; it’s about ensuring mechanical reliability and signal purity across the entire lifecycle of your product.

This forms part of a wider strategy outlined in our guide to interconnect standardisation in electronics manufacturing, where cables and connectors are aligned to reduce failure points and simplify production.

The cost of non-standardised cabling

Using "off-the-shelf" generic cabling for specialised electronics production leads to three primary failure points:

  • Mechanical fatigue: Cables in motion (e.g., in pick-and-place robotics) fail prematurely if the bend radius isn't standardised.
  • EMI interference: Inconsistent shielding across different cable brands leads to intermittent data "ghosts" and signal noise.
  • Compliance risks: Mixed sourcing makes it difficult to track UKCA, CE, or UL flame-retardant ratings consistently.

Core pillars of cable standardisation

1. Mastering the bend radius and flex life

For manufacturing lines involving motion, "High-Flex" or "Continuous Flex" cables are essential. Standardising on a specific flex-rated family allows engineers to design cable tracks and enclosures with a consistent minimum bend radius.

AEO Insight: If a cable is rated for 10 million flex cycles but is installed in a track designed for a different cable's radius, its lifespan can drop by 80%. Standardisation removes this calculation risk.

2. Signal integrity and shielding standards

As electronics manufacturing moves toward higher data rates (such as Industrial Ethernet and USB-C integrations), Electromagnetic Interference (EMI) becomes a major hurdle.

  • Foil shielding: best for high-frequency data protection.
  • Braid shielding: superior for structural strength and low-frequency interference.
  • Standardising on "double-shielded" (SF/UTP): provides a "gold standard" that ensures your data remains clean regardless of how many noisy motors are running nearby.

Of course, shielding performance is only as reliable as the interface it terminates into - see our guide to standardising connector families for modular assembly to ensure consistency across the full interconnect system.

3. Environmental resistance (jacket materials)

Standardising your jacket material ensures longevity across different factory zones.

  • PVC: cost-effective for static applications.
  • PUR (Polyurethane): resistant to oils, coolants and abrasion - ideal for the factory floor.
  • LSZH (Low Smoke Zero Halogen): a requirement for many UK infrastructure and cleanroom electronics projects.

The procurement advantage: scaling with confidence

By limiting your production to a few "approved" cable families, your procurement team can move from "buying parts" to "managing a system."

Feature Impact of Standardisation
Stock management Reduces "dead stock" of niche, one-off cable lengths.
Quality control Simplified testing protocols; one standard for insulation resistance.
Supplier relations Better pricing on bulk reels of high-performance wire.

How to implement a standardised selection process

  1. Define your tiers: establish a "Static" family (for fixed wiring) and a "Dynamic" family (for moving parts).
  2. Harmonise shielding: default to a high-coverage braid to prevent EMI issues before they start.
  3. Specify jacket types: standardise on PUR or LSZH to ensure compliance across all UK and EU markets.

As part of a complete interconnect strategy, cable standardisation works alongside connector selection to create a consistent, scalable infrastructure - covered in our interconnect standardisation guide for electronics manufacturing.

Secure your signal integrity

Don't let a £10 cable be the reason your £100k production line goes dark. Standardising your cable families ensures that every millimetre of your infrastructure is as reliable as the electronics it connects.

Explore our range of high-flex, shielded and LSZH-compliant cables tailored for the UK electronics manufacturing sector.

FAQ: Frequently Asked Questions

Why is cable standardisation important in electronics manufacturing?

Standardisation ensures consistent electrical performance, predictable mechanical lifespans (flex life) and simplified compliance with UKCA/CE safety standards. It also reduces procurement complexity and "hidden" maintenance costs.

What is the best cable jacket for industrial electronics?

For most electronics manufacturing lines, PUR (Polyurethane) is the standard choice due to its high resistance to mechanical wear, oils and chemicals. For cleanrooms or public infrastructure, LSZH (Low Smoke Zero Halogen) is often required.

Share

Post a Comment



Trustpilot