You are using beta.rapidonline.com. For the live site go to rapidonline.com

Thermal imaging cameras for predictive maintenance: what to look for

Published on 10 April 26

Thermal imaging cameras have become a cornerstone of modern predictive maintenance strategies. By allowing engineers and technicians to detect heat anomalies before failures occur, they help reduce downtime, extend asset life and improve safety across industries.

But with a wide range of models and specifications available, choosing the right thermal imaging camera requires more than just comparing price points. This guide outlines what truly matters when selecting a device for reliable, real-world maintenance applications.

Why thermal imaging matters in predictive maintenance

Predictive maintenance relies on identifying early warning signs of equipment failure. Heat is often one of the first indicators of issues such as:

  • Electrical resistance and loose connections
  • Bearing wear and mechanical friction
  • Insulation breakdown
  • Overloaded circuits or components

Thermal imaging enables non-contact, real-time inspection, making it ideal for use in live environments where shutting down equipment is not practical.

Key features to look for

1. Thermal resolution

Resolution determines how much detail the camera can capture.

  • Low resolution (e.g. 80 × 60): Suitable for basic inspections
  • Mid-range (e.g. 160 × 120): Good for general maintenance
  • High resolution (320 × 240 and above): Essential for detailed diagnostics

Higher resolution allows you to detect smaller temperature differences and pinpoint faults more accurately, especially in complex systems like control panels.

2. Temperature range and sensitivity (NETD)

Two critical specifications:

  • Temperature range: Ensure it covers your application (e.g. electrical vs mechanical systems)
  • Thermal sensitivity (NETD): Measures the smallest temperature difference detectable

For predictive maintenance, a low NETD (≤50 mK) is ideal, as it reveals subtle anomalies that may indicate early-stage faults.

3. Accuracy and calibration

Accuracy is vital when decisions are based on temperature readings.

Look for:

  • Accuracy of ±2°C or ±2% of reading
  • Calibration certificates (especially for compliance-heavy industries)

Reliable measurements are essential for trending data over time - a key part of predictive maintenance.

4. Image quality and fusion features

Modern cameras often include:

  • MSX (multi-spectral dynamic imaging) or similar overlay features
  • Visual + thermal image blending
  • Edge enhancement

These features make it easier to interpret images and identify components, especially in busy or complex environments.

FLIR, known for their industry-leading thermal imaging technology and patented MSX® enhancement, are one of the most trusted brands in the thermal imaging sector. Their cameras are widely used across maintenance, engineering and inspection applications, and we’d recommend exploring their range when image clarity, reliability and ease of interpretation are key priorities.

5. Connectivity and data management

Predictive maintenance isn’t just about capturing images, it’s about analysing trends.

Look for:

  • Wi-Fi or Bluetooth connectivity
  • Cloud integration or software compatibility
  • Automated reporting tools

Seamless data transfer helps teams monitor asset health over time and share findings efficiently.

6. Battery life and portability

In real-world maintenance settings, usability matters.

Consider:

  • Battery life (ideally a full working shift)
  • Weight and ergonomics
  • One-handed operation

Technicians often work in confined or elevated spaces, so a lightweight, durable design is essential.

7. Durability and IP rating

Industrial environments can be harsh.

Check for:

  • Drop resistance (e.g. 2 metres)
  • IP rating (IP54 or higher recommended)
  • Operating temperature range

A robust device ensures reliability in environments like factories, outdoor sites and plant rooms.

8. Software and reporting capabilities

A strong software ecosystem enhances the value of your camera.

Key features include:

  • Temperature trend analysis
  • Customisable reports
  • Asset tagging and inspection routes

Good reporting tools support compliance, audits and long-term maintenance planning.

Matching the camera to your application

Not all maintenance tasks require the same level of performance.

  • Electrical inspections: High resolution and sensitivity are critical
  • Mechanical systems: Wider temperature range may be more important
  • Building diagnostics: Focus on image clarity and wide field of view

Understanding your primary use case helps avoid over-specifying or under-specifying your equipment.

Common mistakes to avoid

  • Choosing based on price alone: Lower-cost models may lack the sensitivity needed for predictive work
  • Ignoring software capabilities: Data analysis is just as important as image capture
  • Overlooking training needs: Even the best camera requires proper use to deliver accurate results

In focus

A thermal imaging camera is more than just a diagnostic tool - it’s an investment in reliability, safety and operational efficiency.

When selected carefully, the right device enables maintenance teams to move from reactive fixes to proactive strategies, reducing costly failures and improving overall performance.

Focus on resolution, sensitivity, accuracy, usability and data integration, and you’ll be well-equipped to support an effective predictive maintenance programme.

Share

Post a Comment



Trustpilot