You are using beta.rapidonline.com. For the live site go to rapidonline.com

Where thermistors fit in temperature sensing

Published on 15 January 26

Thermistors occupy a specific but important position in the temperature-sensing landscape. They are not general-purpose sensors for extreme ranges or harsh environments, but within their optimal operating window they offer exceptional sensitivity, fast thermal response and compact integration. Whether utilised as discrete components or integrated into ruggedised thermistor probes, they provide the high-resolution data required for modern electronic control.

As a result, thermistors are frequently chosen where small temperature changes must be detected quickly and accurately, or where temperature sensing and protection need to be embedded directly into an electronic system rather than treated as a standalone measurement function.

How thermistors behave (and why that matters)

Unlike linear sensors such as RTDs, thermistors exhibit a non-linear resistance–temperature relationship. This characteristic is not a drawback by default - it is what gives thermistors their high sensitivity.

The key design question is not “Is a thermistor accurate?” but rather:

Is its response curve suitable for the temperature range and control strategy of the system?

NTC vs PTC: selection by function, not preference

NTC Thermistors – Measurement & control

NTC thermistors reduce resistance as temperature increases. Their steep resistance curve around nominal temperatures makes them highly effective for:

  • Closed-loop temperature control
  • Precision monitoring over narrow ranges
  • Fast detection of thermal changes

Precision thermistors are a subset of NTC devices manufactured with tight resistance and curve tolerances, enabling:

  • Better interchangeability
  • Reduced calibration effort
  • More consistent readings across production batches

They are commonly used in medical devices, instrumentation, and battery management systems.

PTC Thermistors – Protection & safety

PTC thermistors increase resistance as temperature rises, often sharply at a defined threshold.

They are typically specified where the thermistor is expected to:

  • Act as a protective device
  • Limit current automatically
  • Reset once normal conditions return

PTC thermistors are therefore selected less for measurement accuracy and more for predictable, repeatable switching behaviour.

Choosing the correct technology is the first step in designing an effective temperature-sensing circuit. Most applications will utilise either NTC thermistors for linear monitoring or PTC thermistors for safety-critical switching.

When is "Interchangeability" more important than initial tolerance?

In high-volume manufacturing, interchangeability refers to the ability to swap one thermistor for another without recalibrating the entire system. Thermistors are guaranteed to follow a specific resistance-temperature curve within a tight window across a wider band. This reduces labour costs and ensures consistent performance across production batches.

Thermistor probes: When the package is the sensor

A thermistor on its own only measures its own temperature. Thermistor probes exist to ensure that temperature closely represents the target environment, providing the necessary mechanical protection for both NTC thermistors and PTC thermistors in industrial or fluid-based applications.

Probe design affects:

  • Response time
  • Thermal coupling
  • Mechanical durability
  • Long-term stability

Common probe formats include:

  • Stainless steel probes for immersion
  • Epoxy-sealed probes for general-purpose sensing
  • Custom assemblies for OEM equipment

In many applications, probe construction has a greater impact on real-world accuracy than the thermistor element itself.

Accuracy, drift & long-term performance

Tolerance vs real accuracy

Nominal resistance tolerance is only part of the story. System accuracy is influenced by:

  • Curve tolerance (B-value variation)
  • Self-heating from measurement current
  • Thermal contact with the measured medium

Low-cost thermistors may meet initial tolerance specifications but exhibit resistance drift over time, particularly under thermal cycling.

Linearity & signal processing

Because thermistors are non-linear, systems typically rely on:

  • Steinhart–Hart equations
  • Look-up tables
  • Software linearisation

Failing to account for this non-linearity is a common cause of unexpected measurement error, especially when operating outside the intended temperature band.

Environmental & integration considerations

Thermistors are sensitive components and should be evaluated against:

  • Maximum operating temperature
  • Humidity exposure
  • Mechanical strain on leads or probe cables

In harsh environments, thermistors may still be suitable - but only when proper encapsulation and mounting are specified.

How do I protect a thermistor from humidity and corrosive environments?

Thermistors are highly sensitive to moisture, which can bridge the internal conductors and cause a "false low" resistance reading (interpreted as a high temperature). For general use, Epoxy-coated sensors are cost-effective but can eventually absorb moisture. For harsh or high-humidity environments, glass-encapsulated thermistors are essential; they provide a true hermetic seal that prevents drift and protects the delicate ceramic element from chemical attack.

Procurement & specification considerations

For buyers and procurement teams, thermistors present a unique challenge:

  • Many parts share similar headline specifications
  • Performance differences often emerge only over time

Best practice includes:

  • Selecting documented resistance curves
  • Avoiding custom values unless justified
  • Ensuring multi-source availability where possible

Precision thermistors and thermistor probes should be treated as engineered components, not interchangeable commodities.

Closing perspective

Thermistors are deceptively simple components whose real performance depends on curve behaviour, packaging, and system integration rather than nominal resistance alone. By selecting the correct thermistor type (NTC thermistors or PTC thermistors), probe construction, and accuracy class, engineers and buyers can achieve reliable, responsive temperature sensing without unnecessary complexity or cost.

Browse thermistors

FAQs

What are thermistors best used for?

+

Thermistors are best suited to temperature measurement and protection within a defined temperature range where high sensitivity is required.

When should I choose an NTC thermistor?

+

NTC thermistors are preferred for temperature measurement, monitoring, and control applications.

When should I choose a PTC thermistor?

+

PTC thermistors are typically used for overtemperature or overcurrent protection rather than precise measurement.

Are thermistor probes more accurate than bare thermistors?

+

They can be, because controlled packaging improves thermal coupling and repeatability in real-world conditions.

Are thermistors interchangeable?

+

Only if resistance tolerance, curve characteristics, and packaging are tightly controlled.

Share

Post a Comment



Trustpilot