You are using beta.rapidonline.com. For the live site go to rapidonline.com

Why cable shielding matters: EMI, RFI and how to choose the right shield type

Published on 14 April 26

In modern electronic and industrial systems, cables do far more than simply carry power or signals. They operate in environments filled with electrical noise generated by motors, switching power supplies, wireless systems and high-frequency electronics.

Without proper protection, this interference can corrupt signals, disrupt communication systems and even cause equipment failures. That’s why cable shielding plays such a critical role in reliable system design.

In this guide, we’ll explain why cable shielding matters, how electromagnetic interference (EMI) and radio frequency interference (RFI) affect signals, and how to choose the right shielding type for your application.

What is cable shielding?

Cable shielding is a conductive layer surrounding the internal conductors of a cable. Its purpose is to block or reduce unwanted electromagnetic energy that could interfere with signal transmission.

The shield acts as a barrier that either:

  • Reflects external electromagnetic noise, preventing it from reaching the signal wires, or
  • Contains electromagnetic emissions generated by the cable itself.

Properly designed shielding helps maintain signal integrity, improve reliability and support compliance with electromagnetic compatibility standards.

Understanding EMI and RFI

Electromagnetic Interference (EMI)

Electromagnetic Interference (EMI) refers to unwanted electrical noise that disrupts the operation of electronic devices.

Common sources include:

  • Electric motors
  • Switching power supplies
  • Industrial machinery
  • High-power electrical equipment
  • Variable frequency drives

In sensitive electronics, EMI can cause signal distortion, communication errors or unexpected system behaviour.

Radio Frequency Interference (RFI)

Radio-Frequency Interference (RFI) is a specific type of electromagnetic interference occurring within the radio frequency spectrum.

Typical sources include:

RFI is especially problematic for data cables and communication systems where high-frequency signals must remain clean and accurate.

Why cable shielding is important

In industrial and electronic systems, shielding provides several key benefits.

1. Protecting signal integrity

Low-level signals, such as sensor outputs or communication data, are particularly vulnerable to electromagnetic noise.

Shielded cables help maintain clean signals by preventing external interference from coupling into the conductors.

2. Reducing emissions

Cables themselves can act as antennas, radiating electromagnetic energy into the surrounding environment.

Shielding helps contain these emissions and reduces the risk of interfering with nearby equipment.

3. Supporting EMC compliance

Many industries must meet electromagnetic compatibility requirements such as **IEC 61000 standards.

Proper cable shielding helps systems meet these regulations by limiting both emissions and susceptibility to interference.

4. Improving system reliability

Uncontrolled electromagnetic interference can cause:

  • Data corruption
  • Sensor inaccuracies
  • Equipment malfunctions
  • Unexpected system shutdowns

Shielded cables provide an additional layer of protection that improves overall system stability.

Common types of cable shielding

Different shielding methods provide varying levels of protection depending on the application and frequency of interference.

Foil shielding

Foil shielding uses a thin aluminium or copper layer bonded to a film backing.

Advantages

  • Excellent high-frequency protection
  • Lightweight and flexible
  • Provides nearly 100% coverage

Typical applications

  • Data cables
  • Communication systems
  • Control signals

Foil shields are particularly effective at blocking high-frequency interference such as RFI.

Braided shielding

Braided shielding consists of woven strands of copper surrounding the cable conductors.

Advantages

  • High mechanical strength
  • Good low-frequency shielding
  • Flexible and durable

Typical applications

  • Industrial cables
  • Robotics and motion systems
  • Audio and instrumentation cables

Braided shields usually provide 70–95% coverage, depending on the weave density.

Combination shields (foil + braid)

Combination shielding uses both foil and braid to deliver broad‑spectrum interference protection and mechanical resilience.

Advantages

  • High‑frequency protection from foil shielding
  • Low‑frequency shielding and durability from braided shielding

Typical applications

  • Industrial automation
  • High‑performance communication systems
  • Electrically noisy environments

Spiral (serve) shields

Spiral shielding uses helically wrapped copper strands for enhanced flexibility and easier termination.

Advantages

  • Highly flexible
  • Faster and easier to terminate than braided shields

Typical applications

  • Light‑duty or low‑noise installations
  • Applications prioritising flexibility over maximum shielding

Key factors when choosing a shielded cable

Selecting the right cable shielding depends on several practical considerations.

Type of signal

Different signals have different susceptibility to interference.

Examples include:

  • Analogue sensor signals – highly sensitive to noise
  • High-speed data communication – sensitive to RFI
  • Power cables – may require shielding to limit emissions

Understanding signal sensitivity is the first step in choosing appropriate shielding.

Frequency of interference

Shield performance varies with frequency.

  • Foil shields perform well at high frequencies
  • Braided shields perform better at lower frequencies

In mixed environments, combination shielding may provide the best protection.

Environmental conditions

Industrial environments often expose cables to additional stresses such as:

  • Vibration
  • Mechanical movement
  • Oil or chemicals
  • Temperature extremes

In these conditions, braided shields often provide better durability.

Grounding method

Shielding only works effectively when properly grounded.

Incorrect grounding can:

  • Reduce shielding effectiveness
  • Create ground loops
  • Introduce additional noise

In many systems, the shield is grounded at one end only to prevent unwanted current flow.

Common applications that require shielded cables

Cable shielding is especially important in applications such as:

  • Industrial automation systems
  • Robotics and motion control
  • Audio and broadcast equipment
  • Medical devices
  • Data communication networks
  • Instrumentation and measurement systems

In these environments, maintaining clean and reliable signal transmission is critical.

Practical tips for selecting the right shield type

When choosing shielded cables, consider these guidelines:

  • Use foil shielding for high-frequency data signals
  • Use braided shielding for industrial durability
  • Use combination shields in high-noise environments
  • Ensure proper shield grounding and termination
  • Consider flexibility requirements for moving applications

Matching the shield design to the electrical and mechanical demands of the application helps ensure reliable performance.

Select the right shield

Electromagnetic interference is an unavoidable reality in modern electrical and electronic systems. Without proper protection, it can disrupt signals, reduce reliability and compromise system performance.

Cable shielding provides a crucial defence against both EMI and RFI, helping maintain signal integrity and meet regulatory requirements.

By understanding the different shielding types - and selecting the right option for your application, engineers and technicians can ensure their systems operate reliably even in electrically noisy environments.

Popular cable shielding products

Share

Post a Comment



Trustpilot