You are using beta.rapidonline.com. For the live site go to rapidonline.com

Soldering

Soldering is the join at the heart of electronics, and this range covers everything needed to make it well: soldering irons and temperature-controlled stations, solder and flux, desoldering tools, tips and accessories. Rapid supplies the school and college workshop, the maker's bench and the production and repair line alike, from a first learner's iron through to stations for daily professional use.

Choosing soldering equipment

What do I need to start soldering?

At minimum a soldering iron or station, solder, and a way to keep the tip clean; most benches then add a stand, desoldering tool and basic hand tools. A temperature-controlled station is worth it for anything beyond occasional use, as it holds a steady tip temperature for reliable joints. For choosing between models, our guide to soldering equipment walks through what to look for, and the electronic assembly kits range is a good way to practise the skill.

Should I use leaded or lead-free solder?

Lead-free solder is the standard choice for schools and for any RoHS-compliant work, and is the safer option in a teaching environment. Leaded solder is easier to work with at lower temperatures and still used in some repair and specialist contexts. Whichever you choose, good ventilation or fume extraction matters — solder flux fumes should not be breathed in, particularly in a classroom.

Can you supply a classroom, workshop or production line?

Yes. The range runs from class sets of learner irons through to professional stations and the consumables — solder, tips and flux — that all of them get through. Education pricing and class-pack quantities apply for schools and colleges, and bulk ordering keeps a workshop or production line stocked.


Trustpilot