You are using beta.rapidonline.com. For the live site go to rapidonline.com
How cookies can improve your experience
We use cookies on our website to ensure you get the best possible experience – they allow us to tailor content specifically to you, analyse our website to help make improvements, and display ads that are applicable to you across other websites. If you’re happy with this, please select “Allow all", or personalise the cookies you allow with “Manage”. Clicking on “Reject non-essential” will remove these cookies, but the site may not function to its best abilities. For more information, please visit our cookie policy
In industrial automation, robotics and motion control, the terms motor and servo are often used interchangeably, but they shouldn’t be. While both are used to create movement, they differ significantly in control, precision, feedback and application.
Choosing the wrong one can lead to poor performance, wasted energy or unnecessary cost. Choosing the right one can dramatically improve efficiency, accuracy and system reliability.
This guide breaks down the differences clearly, with practical insight into when to use each.
What is a motor?
A motor is a device that converts electrical energy into mechanical motion.
There are many types, but the most common in industrial and commercial use include:
AC motors (induction motors)
DC motors (brushed and brushless)
Most standard motors operate on a simple principle:
Why is closed-loop feedback critical for servo motor precision?
A servo motor achieves accuracy down to fractions of a degree because its internal encoder constantly reports the shaft’s exact physical position back to the controller. If an external load causes a deviation, the system instantly corrects the error. This continuous monitoring makes servos essential for high-dynamic applications like robotic arms, CNC machining and automated pick-and-place systems.
Motors vs servos: the core differences
1. Control system
Motor: open-loop (no feedback)
Servo: closed-loop (constant feedback and correction)
This is the single biggest difference.
2. Precision and accuracy
Motor: limited control over exact position
Servo: highly precise (down to fractions of a degree)
If your application needs exact positioning, a standard motor won’t cut it.
3. Speed and torque control
Motor: basic control via voltage or frequency
Servo: fine-tuned, dynamic control across full range
Servos maintain torque even at low speeds - something many motors struggle with.
4. Complexity
Motor: simple installation and operation
Servo: requires tuning, programming and integration
Servos introduce more setup time but significantly greater capability.
5. Cost
Motor: lower upfront cost
Servo: higher initial investment
However, servos can reduce long-term costs through efficiency, accuracy and reduced waste.
6. Feedback and monitoring
Motor: no inherent feedback
Servo: continuous monitoring of position, speed and torque
This makes servos ideal for smart manufacturing and Industry 4.0 environments.
However, for high-speed, high-precision or high-load environments, servos are typically superior.
Where do stepper motors fit between standard motors and servos?
Stepper motors serve as a middle ground, moving in discrete, fixed angular increments (steps) to provide reliable positional control without requiring an expensive feedback encoder. While simpler and more cost-effective than a servo motor, a stepper motor runs open-loop and can lose its position permanently if the load exceeds its torque capacity, making it best suited for lighter applications like 3D printers.
While standard motors are simpler, servos often provide:
Better energy efficiency (only use power when needed)
Reduced wear due to controlled motion
Less material waste in precision processes
Improved throughput in automated systems
In high-performance environments, these gains can outweigh the higher initial cost.
Final thoughts
The difference between motors and servos comes down to control vs simplicity.
Motors are ideal for straightforward, continuous motion
Servos are essential for precision, responsiveness and intelligent control
As automation, robotics and smart manufacturing continue to evolve, servo systems are becoming increasingly important, but standard motors remain indispensable for simpler, cost-driven applications.
Choosing correctly isn’t about picking the “better” technology - it’s about selecting the right tool for the job.